Setup URSim with Docker

URSim is the offline simulator by Universal Robots. Packed into a remote or virtual machine it acts almost identically to a real robot connected over the network. While it is possible to get URSim running locally on a Linux system or inside a VirtualBox virtual machine, we will focus on getting things setup using Docker. Using Docker for your simulated robot allows you to very quickly spin up a robot testing instance with very little computational overload.

This guide will assume that you have Docker already installed and setup such that you can startup Docker containers using your current user.

The following example will start up a simulator on a UR5e. See the Docker image documentation for more details and configuration options.

Start a URSim docker container

To startup a simulated robot run the following command. This will start a Docker container named ursim and startup a simulated UR5e robot. It publishes ports 5900 and 6080 for VNC / browser-based PolyScope access. Binding those ports to the loopback interface (127.0.0.1) keeps the GUI off your LAN. If you omit the bind address (for example -p 6080:6080), Docker listens on all interfaces and exposes the simulator to the local network unless a firewall prevents that. You can also skip port publishing entirely and reach PolyScope via the container IP, or bind to another interface — including a bracketed IPv6 address such as -p '[::1]:6080:6080'. See Docker’s documentation on publish ports for details.

docker run --rm -it -p 127.0.0.1:5900:5900 -p 127.0.0.1:6080:6080 --name ursim universalrobots/ursim_e-series

With the loopback binds above, open http://127.0.0.1:6080/vnc.html (or connect a VNC client to 127.0.0.1:5900) on the Docker host.

External Control

To use the external control functionality, we will need the external_control URCap installed on the robot and a program containing its ExternalControl program node. Both can be prepared on the host machine either by creating an own Dockerfile containing those or by mounting two folders containing installed URCaps and programs. See the Docker image documentation.

In this example, we will bind-mount a folder for the programs and URCaps. First, let’s create a local folder where we can store things inside:

mkdir -p ${HOME}/.ursim/programs
mkdir -p ${HOME}/.ursim/urcaps

Then, we can “install” the URCap by placing its .jar file inside the urcaps folder

URCAP_VERSION=1.0.5 # latest version as if writing this
curl -L -o ${HOME}/.ursim/urcaps/externalcontrol-${URCAP_VERSION}.jar \
  https://github.com/UniversalRobots/Universal_Robots_ExternalControl_URCap/releases/download/v${URCAP_VERSION}/externalcontrol-${URCAP_VERSION}.jar

With this, start your URSim containers with the following command:

docker run --rm -it -p 127.0.0.1:5900:5900 -p 127.0.0.1:6080:6080 -v ${HOME}/.ursim/urcaps:/urcaps -v ${HOME}/.ursim/programs:/ursim/programs --name ursim universalrobots/ursim_e-series

With this, you should be able to setup the external_control URCap and create a program as described in URCap setup guide.

Network setup

As described above, you can always start the URSim container using the default network setup. It will most probably always get the same IP address assigned every time, as long as you don’t have any other docker containers running. However, to make things a bit more explicit, we can setup our own docker network where we can assign a static IP address to our URSim container.

docker network create --subnet=192.168.56.0/24 ursim_net
docker run --rm -it -p 127.0.0.1:5900:5900 -p 127.0.0.1:6080:6080 --net ursim_net --ip 192.168.56.101 universalrobots/ursim_e-series

The above commands first create a network for docker and then create a container with the URSim image attaching to this network.

With a fixed container IP you can also skip publishing the GUI ports and open http://192.168.56.101:6080/vnc.html when the browser can reach that address (typically when Docker and the browser run on the same host). Published ports remain useful behind Docker Desktop / NAT, or when you deliberately bind only to loopback / a specific interface.

Script startup

All of the above is put together in a script in the ur_client_library package.

By default, start_ursim.sh:

  • Attaches the container to ursim_net at 192.168.56.101

  • Publishes the robot interface ports (30001-30004, and 29999 for CB3 / PolyScope 5)

  • Publishes the GUI on loopback only: VNC 127.0.0.1:5900 / 127.0.0.1:6080 (CB3 / PolyScope 5), or the PolyScope X web UI at 127.0.0.1:8000 (container port 80)

After startup, the script prints both the container-IP URLs and the host endpoints taken from docker port for any published GUI ports. Override publishing with -f (pass DISABLED to turn it off). Examples:

# Custom host ports on all interfaces
./scripts/start_ursim.sh -f "-p 30001-30004:30001-30004 -p 16080:6080 -p 15900:5900"

# Bind GUI ports to IPv6 loopback (keep the -f argument in double quotes)
./scripts/start_ursim.sh -f "-p 30001-30004:30001-30004 -p [::1]:6080:6080 -p [::1]:5900:5900"

# Extra docker run options, such as another volume or environment variable.
# Keep the -a argument in double quotes; it is split on whitespace.
./scripts/start_ursim.sh -a "-v /tmp/data:/data -e FOO=bar"
rosrun ur_client_library start_ursim.sh

This will start a URSim docker container running on 192.168.56.101 with the external_control URCap preinstalled. Created programs and installation changes will be stored persistently inside ${HOME}/.ursim/programs.

With this, you can run

roslaunch ur_robot_driver ur5e_bringup.launch robot_ip:=192.168.56.101

Using another registry or image

By default the script starts universalrobots/ursim_<series>:<version>. -r <registry> replaces the universalrobots prefix. A trailing slash is stripped. The container keeps the tag you requested. If that image is already available locally, its URSim version label is still used for the version checks and setup:

./scripts/start_ursim.sh -r registry.example.com/ur -v 5.21.0

-I <image[:tag]> uses that image as given. -m and -v still select the robot series, the version checks, the volume mounts and the environment variables. -I takes precedence over -r. The version label inside an arbitrary image is not inspected.

./scripts/start_ursim.sh -I registry.example.com/robots/custom-ursim:latest -m ur10g-1750 -v 10.15.0