You're reading the documentation for an obsolete version. For the latest released version, please have a look at mp1.4.
MotionPlus URCap Errors
This page describes the public error codes generated by the EtherCAT URCap and reported directly to the user via URScript popups.
It does not describe the various internal error codes which may be reported in the EtherCAT Daemon log file. These error codes are not fixed as they are generated by various software components, many of which are maintained separately from the URCap.
Error Categories
Each public error code for the EtherCAT URCap falls under one of the following categories, according to the value of the error code:
| Error Range | Category | Description | 
|---|---|---|
| 0 | Success | indication that no error has occurred | 
| 100-199 | XML-RPC client | any error generated when client passes an invalid argument to XML-RPC method or fails to meet one of the method’s preconditions | 
| 200-299 | XML-RPC service | any error generated during the execution of an XML-RPC method (with valid arguments and its preconditions met) | 
| 300-399 | EtherCAT master | any error generated by the EtherCAT master (after it has been configured and started)NOTE: Each of these errors will cause the EtherCAT master to halt and will prevent it from being restarted until the error is cleared. (See “Error Display” section of URCap Installation Page Documentation for more information.) | 
100-199 XML-RPC client errors
| Code | Name | Description | Corrective Action | 
|---|---|---|---|
| 101 | Invalid Network Interface | Given device name references a network device that does not exist or is unsuitable for EtherCAT communication. | Try again with a supported device name. | 
| 102 | Invalid Axis Index | Given axis index is negative or larger than the maximum supported axis index. | Try again with a valid axis index. | 
| 103 | Duplicate Axis Config | Given axis configuration has an axis index, axis name, or station address that is already in use by another existing axis configuration. | Try again with axis index, axis name, and station address values that are not already in use. | 
| 104 | No Network Interface Selected | No network device has been selected for EtherCAT communication. | Select an EtherCAT network device and try again. | 
| 105 | No Axes Configured | No axes have been configured for the EtherCAT master. | Define one or more axes configurations and try again. | 
| 106 | Master Halted from Error | EtherCAT master has halted due to a runtime error and cannot be restarted until error has been cleared. | Inspect Error Display on URCap Installation Page to determine which runtime error has occurred. Then look up the runtime error in the EtherCAT Master Errors section of this document and perform the recommended corrective action. | 
| 107 | Master Already Running | An attempt was made to start the EtherCAT master while it was already running. | Stop the EtherCAT master and try again. | 
200-299 XML-RPC service errors
| Code | Name | Description | Corrective Action | 
|---|---|---|---|
| 201 | Internal Service Error | An internal error (e.g. software bug) occurred during execution of the XML-RPC method. | Reattempt operation. If problem persists, contact UR with error details from EtherCAT daemon log file. | 
| 202 | Network Interface Enable Failed | Network device selected for EtherCAT communication could not be enabled. | Select a different network device and reattempt operation. If problem persists, contact UR with error details from EtherCAT daemon log file. | 
| 203 | Master Start Failed | An error occurred while starting the EtherCAT master. | Verify  | 
300-399 EtherCAT master errors
| Code | Name | Description | Corrective Action | 
|---|---|---|---|
| 301 | Internal Master Error | EtherCAT master has encountered an internal error (e.g. software bug). | Clear the error and restart the master. If problem persists, contact UR with error details from EtherCAT daemon log file. | 
| 302 | Missing URControl Feedback | EtherCAT master has no realtime communication with UR Controller. | Verify UR Controller is running and is not in a fault state. Then clear error and restart EtherCAT master. | 
| 303 | Master State Update Failed | EtherCAT master failed to reach target state (e.g. OP) within expected deadline. | Verify UR control box and all expected EtherCAT slaves are connected to the EtherCAT network. Also verify all EtherCAT slaves are powered on. Finally clear error and restart EtherCAT master. | 
| 304 | EtherCAT Send Failed | EtherCAT master failed to send data over EtherCAT network. | Verify UR control box and all expected EtherCAT slaves are connected to the EtherCAT network. Also verify all EtherCAT slaves are powered on. Finally clear error and restart EtherCAT master. | 
| 305 | EtherCAT Receive Failed | EtherCAT master failed to receive data over EtherCAT network. | Verify UR control box and all expected EtherCAT slaves are connected to the EtherCAT network. Also verify all EtherCAT slaves are powered on. Finally clear error and restart EtherCAT master. | 
| 306 | Slave Command Failed | EtherCAT slave failed to process command word within expected deadline. | Verify slave is not in fault sate. Then clear error and restart EtherCAT master. |