MotionPlus Documentation Logo

Contents

  • MotionPlus Introduction
  • MotionPlus URCap
  • Servo Setup and Test
  • Servo Troubleshooting
  • URScript APIs
  • World Model
  • URScript Examples
    • MotionPlus
      • Constructing and Jogging a Single Axis Positioner
      • Constructing the Kinematics of a Two Axis Positioner
      • Jogging Two Axis Groups Using Threads
      • Attaching Frames to An Axis
      • Basic Frame Tracking with an Axis
      • Programming Waypoints in a Moving Frame
      • Coordinated Motion with an Axis
      • Manually Setting the Axis Indices and Streaming over RTDE
      • Configuring, Enabling, and Driving EtherCAT Axes
    • World Model
      • Adding, Moving, and Attaching Frames
      • Moving the Robot Using Frames
      • Moving the Robot Relative to the TCP
      • Moving the Robot’s Base While Following A Trajectory
  • MotionPlus URCap Errors
  • FAQ - Frequently Asked Questions
  • Release Notes
MotionPlus Documentation
  • URScript Examples

You're reading the documentation for an obsolete version. For the latest released version, please have a look at mp1.5.

URScript Examples

MotionPlus

  • Constructing and Jogging a Single Axis Positioner
  • Constructing the Kinematics of a Two Axis Positioner
  • Jogging Two Axis Groups Using Threads
  • Attaching Frames to An Axis
  • Basic Frame Tracking with an Axis
  • Programming Waypoints in a Moving Frame
  • Coordinated Motion with an Axis
  • Manually Setting the Axis Indices and Streaming over RTDE
  • Configuring, Enabling, and Driving EtherCAT Axes

World Model

  • Adding, Moving, and Attaching Frames
  • Moving the Robot Using Frames
  • Moving the Robot Relative to the TCP
  • Moving the Robot’s Base While Following A Trajectory
Previous Next

© Copyright 2025, Universal Robots A/S.

Other Versions v: mp1.1
Branches
mp1.5
mp1.0
mp1.1
mp1.2
mp1.3
mp1.4