You're reading the documentation for an obsolete version. For the latest released version, please have a look at mp1.5.
Servo Setup and Test
Overview
This document is intended to guide UR+ partners and Certified Systems Integrators (CSI) in the setup of a single servo drive for external rotary axis. The intended application is to drive a rotary part positioner in coordinated motion for welding.
Steps
The steps listed below, in order, are covered in this document.
Install the MotionPlus URCap
Set up the servo drive and motor with appropriate power
Connect the servo drive to the UR Controller
Power up the servo drive
Start the MotionPlus service
Modify the ServoConfig script
Run ServoTests 1,2, 3 and 4
Install the MotionPlus URCap
The MotionPlus EtherCAT master is contained in the MotionPlus URCap. It communicates with the the UR Controller over shared memory to send external axis positions from the controller to the EtherCAT drives at 2ms intervals - following the 500Hz clock cycle of the UR controller.
Install the URCap using a USB thumbdrive inserted into the teach pendant. For more information on installing URCaps in general, please refer to this page: Installing a URCap or this page specifically for MotionPlus URCap installation.
Tested Servos
We have tested the following servo drives for MotionPlus compatibility in our lab:
Festo Servo Drive CMMT-AS/CMMT-ST
HCFA Y7S
Innovance SV660N
Kollmorgen AKD2G Series
Mitsubishi J4 and J5 Series
Nanotec PD4
Oriental Motor AZD-AED, AZXD-SED
Sanyo Denki SANMOTION G
Yaskawa Sigma7
EtherCAT and USB Ethernet Adapters
Note
We no longer recommend using an USB-Ethernet adapter for EtherCAT due to communication stability problems. Only the use of the control box primary ethernet port is supported for EtherCAT. Do not connect your EtherCAT cable to a network switch - it should be connected directly from the control box to the first EtherCAT servo drive on the fieldbus.
EtherCAT requires very stable communications with low latency and minimum jitter. That is not easily obtained with a USB Ethernet Adapter. For this reason, we only support EtherCAT communication over the primary ethernet port (RJ45 connector).
You may still want to use an ethernet adapter to communicate with the robot over TCP/IP, for example using ssh. In this case, you can use supported USB Ethernet Adapters:
TP Link UE300 (version 4.6 or earlier)
The UE300 is supported up to Version 4.6. Check the label on the USB adapter. If it is v5.0 or later, it is not yet supported with the UR kernel drivers.
Ethernet Port Swap
The MotionPlus URCap is configured to communicate via EtherCAT on the eth1 interface, while Polyscope is configured to communicate TCP/IP on the eth0 interface. MotionPlus requires the underlying hardware to be swapped: eth1 to use the built-in ethernet port and eth0 to use a USB-Ethernet Adapter. Please refer to to the Ethernet Port Swap page.
Setup the Servo Drive
Verify that your servo drive supports the necessary protocol. The drive should be capable of;
EtherCAT communication
DC - Distributed Clock
Cia402 Motion Control Profile
CSP - Cyclic Synchronous Positioning (mode 8)
Adjustable cycle time to 2ms (most drives offer this with options for 1ms, 2ms, 4ms)
E-Stop input, optional but recommended. Should be wired in with the UR Control E-Stop safety I/O.
Once you verify that the drive meets this criteria, check for the following capabilities of your servo motor:
Motor has a positioner encoder (absolute or relative). If relative, homing will be required.
Motor has brakes to stop the rotary positioner from moving when power is removed.
Your servo drive should be securely mounted to a fixed base for testing. The shaft (with or without gearbox) should be able to turn freely. Do not attach any load to the drive for these early tests. A qualified technician should connect the drive to its power source, ensure appropriate grounding, and provide the appropriate DC power source for the drive electronics. UR does not provide support or guidance in the installation and wiring of servo drives - please consult with your distributor or servo drive manufacturer.
Connect to the Servo Drive
The UR Control Box (series 5.x) should be connected to the servo drive using an ethernet cable. This cable can be a standard Cat5e cable with RJ45 connectors, or the cable provided by the servo drive manufacturer. Do not connect EtherCAT through a network switch. It should be connected directly to the first servo drive in the EtherCAT chain.
Power Up the Servo Drive
Apply the mains (AC) and the DC power to the servo drive. The Servo Drive should come up, ready to connect. If the servo drive display shows a fault, this must be resolved before proceeding further. For example, some servos require that you clear the encoder backup fault if you have had the drive stored and without power for some time.
Configure the Servo Drive
You will need to have your manfuacturer’s configuration software to set up the servo drive. The typical parameters to set are:
Cycle Time (should be set to 2ms)
Position Base Unit (should be set to radians for rotary and meters for linear axes)
Feed Constant
Gear Ratio
Encoder Resolution
For more information on the specific EtherCAT parameters to set in your configuration software please refer to Servo Configuration
Warning
In order to avoid overflow of the position value (int32), we recommend that you set up your servo drive position units in radians for rotary and in meters for linear axes. Using units of encoder counts can cause overflow in set-ups with high gear ratio (>100:1).
Start the MotionPlus Service
In Polyscope, on the installation page, click on the side tab for MotionPlus. Select the network device from the drop down list, choosing eth1 as your device of choice. Click the [Start] button to begin the MotionPlus service. This starts the service but does not start the EtherCAT master. That is done using a URScript command in the upcoming steps.
Modify the MotionPlus Servo Config Script
See the examples.
Note
It is assumed that you have used your manufacturer’s software to configure units for position in this previous section: Configure The Servo Drive
You must first copy and modify this script to match your particular servo drive.
Set the value for your encoder resolution (counts per revolution). It’s important to get this right as it affects the positioning and speed of the motor turning
Set the value for the feed constant to 2*PI for a rotary axis if not already set. You may have to changes the sign (+/-) later to ensure that the motor turns in the proper direction.
Set the axis type to revolute if not already set.
Save your changes to the servoconfig script.
Servo Tests Program Setup
Create a new program
Turn off the ‘Loop forever’ option
Add the servo config script
Add the servo test scripts 1, 2, 3 and 4 from the following sections
Turn off scripts 2, 3 and 4. We will only run one test at a time, disabling the others while we run.
Servo Test 1 - Basic Servo Move
See the examples.
This first test will check to see if the ethercat communications are working and that the servo motor can rotated one turn in each direction, with a speed of 1 revolution per second.
Power up the robot from the Teach Pendant (main screen, lower left button)
Run the program
You should see the motor rotate one turn counter clockwise (view facing the end of the motor shaft our gear output), then rotate two turns clockwise, and finally rotate back to the starting position.
The speed should be 1 revolution per second.
If the motor rotates in the opposite direction, then edit the your servo script and change the sign for the feedconstant to -2*PI.
If the motor rotates faster or slower than expected it is possible that you have the wrong setting for encoder counts-per-revolution. Check your servo motor manual and consult with your servo manufacturer.
If the servo drive issues a fault or the MotionPlus displays and error, please consult the MotionPlus TroubleShooting (document)[servotrouble.md] for diagnostic techniques.

Servo Test 2 - Homing
See the example.
Once you have completed Test #1, you are ready to test homing. MotionPlus (release 1.0) only supports homing at the current position. This effectively resets the internal encoder count to zero immediately without moving the motor. More advanced homing techniques with limits switches are coming in a later update to MotionPlus.
Power up the robot from the Teach Pendent (main screen, lower left button)
Disable Servo Test1 and enable Servo Test 2
Run the program
The homing test is in two parts. The first is without homing, then the same motion executed with homing.
For the first part, you should see the motor perform three revolutions - rewinding to zero after each turn.
In the second part, the program will home to zero between revolutions, so there should be no rewind - just three revolutions in the same direction with a pause of 1 sec between each one.
Servo Test 3 - Calibration
See the example scripts for single-axis and dual-axis calibration.
In order to perform coordinated motion, we need to calibrate the pose of the rotary axis with respect to the robot base pose. This is done through a calibration procedure. Follow these steps:
Power on the robot
Attach a pointing tool (see image below) for the calibration procedure.
Use the built-in Polyscope TCP calibration to create a TCP for the pointing tool.
Set the TCP for the pointer as default.
Add an installation variable named CAL_AX1_ROTARY and set the value to p[0,0,0,0,0,0]. This global installation variable will store the calibration pose for the rotary axis.
On the program tab, disable Servo Test 2 and enable Servo Test 3
Run the program

This program will instruct you to teach a single point in four different positions on the circumference of a circle around the motor shaft center. You will need to identify a single feature that rotates around the axis as the teachable point. The axis will start at position 0, and then increment 90 degrees for each additional point to teach. The four sampled points are used to calculate the position and orientation of the axis of rotation.
The result is the pose update of the global variable CAL_AX1_ROTARY, used in the next step for testing coordinated motion.
Servo Test 4 - Coordinated Motion
See the example script.
This final step will test motion of the robot TCP and the rotary axis together. This test is quite simple - the robot TCP, close to the rotary axis will synchronize with the motion of the axis - appearing to remain fixed to the rotary direction. In this test, we command the robot TCP to frame track with the axis, then we turn the axis. We do not directly command the robot position. This is a visual verification to check if your servo config is also correct and that you have calibrated the axis accurately.
Power on the robot
Disable Servo Test 3 and enable Servo Test 4
Using Free Drive, bring the robot TCP close but not touching the motor shaft or attached flange. A distance of 5-10cm is suggested.
Adjust the speed slider on the Teach Pendant down to 10%
Be ready to stop the program immediately if the robot moves in the wrong direction - i.e. does not follow the axis rotation direction.
Run the program
First, the servo should turn a quarter turn in the positive direction (90 degrees), back to the starting position, then a quarter turn in the negative direction (-90 degrees), then back to start.
Next, with tracking on, this motion is repeated, but this time with the TCP pointer tracking the rotary motion.
Important
If the robot moves in the wrong direction with tracking on, then the calibration routine from the previous step was not successful and needs to be performed again with careful attention being made to the order in which the calibration points are taught according to the right-hand rule.