TCP/IP Socket Communication via URScript with Universal Robots
Universal Robots provides an efficient method for establishing TCP/IP socket communication between a UR robot and external equipment. This guide demonstrates how to set up the robot as a client using URScript, communicating with a server (a PC in this case).
Server Setup
A C# console application, built using Visual Studio 2010, acts as the server. The server listens for connections on IP 127.0.0.1 and port 21. The following steps outline the server setup:
Initialize Server:
IPAddress ipAddress = IPAddress.Parse("127.0.0.1"); TcpListener tcpListener = new TcpListener(ipAddress, 21); tcpListener.Start();
Accept Connections:
TcpClient tcpClient = tcpListener.AcceptTcpClient(); NetworkStream stream = tcpClient.GetStream();
Handle Client Requests:
while (tcpClient.Client.Connected) { byte[] arrayBytesRequest = new byte[tcpClient.Available]; int nRead = stream.Read(arrayBytesRequest, 0, arrayBytesRequest.Length); if (nRead > 0) { string sMsgRequest = ASCIIEncoding.ASCII.GetString(arrayBytesRequest); // Process the request and send a response } }
Client Setup in URScript
The UR robot is programmed to act as a client, connecting to the server and exchanging data. Here is a basic URScript example for the client:
Open Socket:
open≔socket_open("127.0.0.1",21) Loop open=False open≔socket_open("127.0.0.1",21)Send Data:
sendToServer≔'send to server' socket_send_string(sendToServer)
Receive Data:
receiveFromServ≔socket_read_ascii_float(6) Loop receiveFromServ[0]≠6 Wait: 0.3 receiveFromServ≔socket_read_ascii_float(6)
Move Robot Based on Received Data:
Loop counter<6 targetPos[counter]=receiveFromServ[counter+1] counter≔counter+1 MoveJ targetPos
Data Format Requirements
When using socket_read_ascii_float in URScript, ensure that:
Data is surrounded by parentheses.
Each data unit is separated by a comma.
The message ends with
\n.
Example:
Server sends:
"(0.4, 0, 0.5, 0, -3.14159, 0)\n".Client receives:
[6,0.4, 0, 0.5, 0, -3.14159, 0].
For more details and to download the necessary files, visit the Universal Robots TCP/IP socket communication guide.