Primary and Secondary Interfaces

The UR controller provides servers that send robot state data and receive URScript commands. The primary interface transmits robot state data and additional messages. The secondary interface transmits robot state data only. The data is mainly used for communication between the GUI and the controller. Both accept URScript commands with state data updates at a 10 Hz rate. This makes it possible to control the robot remotely with a dynamically generated robot program.

TCP ports used by interfaces

  • Primary client: port 30001 (Robot state and messages)

  • Secondary client: port 30002 (Only robot state and the Version messages)

  • Primary client read only: port 30011 (Robot state and messages)

  • Secondary client read only: port 30012 (Only robot state and the Version messages)

Messages

Data sizes

Data Type

Size

int16_t

2 bytes

int32_t

4 bytes

float

4 bytes

double

8 bytes

bool

1 byte

uint8_t

1 byte

Array notation is used where the same type is repeated several times.

Example of fixed-length array: double DHa[6] — 6 doubles, 48 bytes total.

Example of variable-length array: char buildData[] — either the length is given as one of the fields, or the data spans until the end of the package.

Commands sent to Primary and Secondary interfaces

The primary interface accepts script commands. Typically, commands are aggregated into a complete program.

If remote control is intended to dynamically control part of the trajectory, it is recommended to use Interpreter Mode instead. Refer to the Script Manual for more information.

NOTE: Commands not documented in the Script Manual are used internally by UR software and are not backwards compatible.

Status messages sent to clients

All messages and sub-packages contain a length field at the beginning, followed by a type field.

NOTE: Future Polyscope versions may add additional fields to existing messages or sub-message types. Client code should be able to interpret partial messages and ignore the remaining data. Deprecated and reserved fields should not be used, as they can change content in future software releases.

Robot State Message

This message is sent periodically and contains multiple sub-packages.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_ROBOT_STATE = 16

Sub packages

One or more sub packages. Each contains size, type, and package specific data

Robot Mode Data (Sub Package of Robot State Message)

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

uint8_t packageType

ROBOT_STATE_PACKAGE_TYPE_ROBOT_MODE_DATA = 0

uint64_t timestamp

Microseconds since controller started

bool isRealRobotConnected

bool isRealRobotEnabled

bool isRobotPowerOn

bool isEmergencyStopped

bool isProtectiveStopped

bool isProgramRunning

bool isProgramPaused

uint8_t robotMode

Robot Modes

uint8_t controlMode

Control Modes

double targetSpeedFraction

double speedScaling

double targetSpeedFractionLimit

uint8_t reserved

Internal use only

Joint Data (Sub Package of Robot State Message)

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

uint8_t packageType

ROBOT_STATE_PACKAGE_TYPE_JOINT_DATA = 1

Following 8 fields are repeated for each joint (6 times)

→ double q_actual

→ double q_target

→ double qd_actual

→ float I_actual

→ float V_actual

→ float T_motor

→ float reserved

Deprecated — ignore

→ uint8_t jointMode

Joint Modes

Tool Data (Sub Package of Robot State Message)

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

uint8_t packageType

ROBOT_STATE_PACKAGE_TYPE_TOOL_DATA = 2

uint8_t analogInputRange0

uint8_t analogInputRange1

double analogInput0

double analogInput1

float toolVoltage48V

uint8_t toolOutputVoltage

float toolCurrent

float toolTemperature

uint8_t toolMode

Tool Modes

Masterboard Data (Sub Package of Robot State Message)

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

uint8_t packageType

ROBOT_STATE_PACKAGE_TYPE_MASTERBOARD_DATA = 3

uint32_t digitalInputBits

uint32_t digitalOutputBits

uint8_t analogInputRange0

uint8_t analogInputRange1

double analogInput0

double analogInput1

char analogOutputDomain0

char analogOutputDomain1

double analogOutput0

double analogOutput1

float masterBoardTemperature

float robotVoltage48V

float robotCurrent

float masterIOCurrent

uint8_t safetyMode

Subset of Safety Modes

bool inReducedMode

bool immiInterfaceInstalled

True if the IMMI interface is installed

Following 4 fields are present only if immiInterfaceInstalled is true

→ uint32_t immiInputBits

→ uint32_t immiOutputBits

→ float immiVoltage24V

→ float immiCurrent

uint32_t reserved

Used by Universal Robots software only

uint8_t operationalModeSelectorInput

bool threePositionEnablingDeviceInput

uint8_t safetyStatus

Safety status

Cartesian Info (Sub Package of Robot State Message)

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

uint8_t packageType

ROBOT_STATE_PACKAGE_TYPE_CARTESIAN_INFO = 4

double X

double Y

double Z

double Rx

double Ry

double Rz

double TCPOffsetX

double TCPOffsetY

double TCPOffsetZ

double TCPOffsetRx

double TCPOffsetRy

double TCPOffsetRz

Kinematics Info (Sub Package of Robot State Message)

This information is sent upon leaving initialization mode and when the kinematics configuration has changed.

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

uint8_t packageType

ROBOT_STATE_PACKAGE_TYPE_KINEMATICS_INFO = 5

uint32_t checksum[6]

double DHtheta[6]

double DHa[6]

double DHd[6]

double DHalpha[6]

uint32_t calibrationStatus

Configuration Data (Sub Package of Robot State Message)

This information is sent once after the client connection is established.

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

uint8_t packageType

ROBOT_STATE_PACKAGE_TYPE_CONFIGURATION_DATA = 6

Following 2 fields are repeated for each joint (6 times)

→ double jointMinLimit

→ double jointMaxLimit

Following 2 fields are repeated for each joint (6 times)

→ double jointMaxSpeed

→ double jointMaxAcceleration

double vJointDefault

double aJointDefault

double vToolDefault

double aToolDefault

double eqRadius

double DHa[6]

double Dhd[6]

double DHalpha[6]

double DHtheta[6]

int32_t masterboardVersion

int32_t reserved

Deprecated in 5.26.0 / 10.13.0

int32_t robotType

Robot Arm type

int32_t robotSubType

uint16_t controlboxType

Control Box Type

5.26.3 / 10.15.0

uint16_t toolFlangeType

Tool Flange Type

5.26.3 / 10.15.0

NOTE: The controlboxType and toolFlangeType fields were introduced in 5.26.0 / 10.13.0, but their values were not stable until 5.26.3 / 10.15.0.

Force Mode Data (Sub Package of Robot State Message)

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

uint8_t packageType

ROBOT_STATE_PACKAGE_TYPE_FORCE_MODE_DATA = 7

double Fx

Deprecated — always contains the value 0.0

double Fy

Deprecated — always contains the value 0.0

double Fz

Deprecated — always contains the value 0.0

double Frx

Deprecated — always contains the value 0.0

double Fry

Deprecated — always contains the value 0.0

double Frz

Deprecated — always contains the value 0.0

double robotDexterity

Additional Info (Sub Package of Robot State Message)

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

uint8_t packageType

ROBOT_STATE_PACKAGE_TYPE_ADDITIONAL_INFO = 8

uint8_t tpButtonState

bool isManualFreedriveAllowed

bool isFreedriveIOPressed

uint8_t tpType

Teach Pendant Type

Calibration Data (Sub Package of Robot State Message, Internally Used Only)

This sub-package is used internally by UR software and should be ignored.

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

uint8_t packageType

ROBOT_STATE_PACKAGE_TYPE_CALIBRATION_DATA = 9

uint32_t reserved

Used by Universal Robots software only

Safety Data (Sub Package of Robot State Message)

This sub-package is used internally by UR software and should be ignored.

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

unsigned char packageType

ROBOT_STATE_PACKAGE_TYPE_SAFETY_DATA = 10

reserved

Used by Universal Robots software only

Tool Communication Info (Sub Package of Robot State Message)

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

unsigned char packageType

ROBOT_STATE_PACKAGE_TYPE_TOOL_COMM_INFO = 11

bool toolCommunicationIsEnabled

int32_t baudRate

int32_t parity

int32_t stopBits

float RxIdleChars

float TxIdleChars

Tool Mode Info (Sub Package of Robot State Message)

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

unsigned char packageType

ROBOT_STATE_PACKAGE_TYPE_TOOL_MODE_INFO = 12

uint8_t outputMode

uint8_t digitalOutputModePin0

uint8_t digitalOutputModePin1

Singularity Info (Sub Package of Robot State Message)

This sub-package is used internally by UR software and should be ignored. Package is sent only when robot is in freedrive mode with individual lockable axes.

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

unsigned char packageType

ROBOT_STATE_PACKAGE_TYPE_SINGULARITY_INFO = 13

uint8_t singularitySeverity

uint8_t singularityType

Payload Info (Sub Package of Robot State Message)

This sub-package is used internally by UR software and should be ignored.

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

unsigned char packageType

ROBOT_STATE_PACKAGE_TYPE_ACTIVE_PAYLOAD = 14

reserved

Used by Universal Robots software only

Internal Data (Sub Package of Robot State Message)

This sub-package is used internally by UR software and should be ignored.

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

unsigned char packageType

ROBOT_STATE_PACKAGE_TYPE_INTERNAL_DATA = 15

reserved

Used by Universal Robots software only

Cumulative Runtime Data (Sub Package of Robot State Message)

Message is sent once per second.

Field

Description

Introduced in version

uint32_t packageSize

Total length of subpackage including this field

5.23.0 / 10.11.0

unsigned char packageType

ROBOT_STATE_PACKAGE_TYPE_CUMULATIVE_RUNTIME_DATA = 16

5.23.0 / 10.11.0

double robot_energy_consumed_Wh

Robot Arm energy consumption since controller startup [Wh].

5.23.0 / 10.11.0

double robot_braking_energy_dissipated_Wh

Robot Arm braking energy dissipated since controller startup [Wh].
This energy is flowing back into the Control Box and gets dissipated as heat.

5.23.0 / 10.11.0

Robot Message

There are several messages grouped under the “Robot Message” type. Note that sub-messages don’t contain their own size field; only the main message does. Each complete message contains exactly one sub-message.

Some messages are sent only to Primary Interface clients.

Version Message

This is the first package sent on both the primary and secondary client interfaces. Package is sent only once.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_ROBOT_MESSAGE = 20

uint64_t timestamp

Microseconds since controller started

int8_t source

Message Sources

char robotMessageType

ROBOT_MESSAGE_TYPE_VERSION = 3

char projectNameSize

char projectName[]

uint8_t majorVersion

uint8_t minorVersion

int32_t bugfixVersion

int32_t buildNumber

char buildDate[]

HardwareInfoMessage

Package is sent only once.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_ROBOT_MESSAGE = 20

uint64_t timestamp

Microseconds since controller started

int8_t source

Message Sources

char robotMessageType

ROBOT_MESSAGE_TYPE_HARDWARE_INFO = 18

int32_t robotType

Robot Arm type

5.26 / 10.14

uint16_t reserved

reserved for future protocol extensions

uint16_t controlboxType

Control Box Type

5.26.3 / 10.15.0

uint16_t reserved

reserved for future protocol extensions

uint16_t toolFlangeType

Tool Flange Type

5.26.3 / 10.15.0

NOTE: The controlboxType and toolFlangeType fields were introduced in 5.26.0 / 10.14.0, but their values were not stable until 5.26.3 / 10.15.0.

Safety Mode Message

The message is sent only to Primary Interface clients.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_ROBOT_MESSAGE = 20

uint64_t timestamp

Microseconds since controller started

int8_t source

Message Sources

uint8_t robotMessageType

ROBOT_MESSAGE_TYPE_SAFETY_MODE = 5

int32_t robotMessageCode

int32_t robotMessageArgument

uint8_t safetyModeType

Safety Mode Types

uint32_t reportDataType

Following data type depends on this value

0,1:uint32_t
2:int32_t
3:float
4:uint32_t that should be displayed as HEX

→ type32 reportData

Robot Comm Message

The message is sent only to Primary Interface clients.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_ROBOT_MESSAGE = 20

uint64_t timestamp

Microseconds since controller started

int8_t source

Message Sources

uint8_t robotMessageType

ROBOT_MESSAGE_TYPE_ERROR_CODE = 6

uint32_t robotMessageCode

uint32_t robotMessageArgument

int32_t robotMessageReportLevel

Report Levels

uint32_t dataType

Following data type depends on this value

0,1:uint32_t
2:int32_t
3:float
4:uint32_t that should be displayed as HEX

→ type32 reportData

5:String

→ uint16_t textLength

→ char textMessage[]

Last field is 32-bit number for dataType (0-4) or variable length string for dataType 5.

Key Message

The message is sent only to Primary Interface clients.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_ROBOT_MESSAGE = 20

uint64_t timestamp

Microseconds since controller started

int8_t source

Message Sources

uint8_t robotMessageType

ROBOT_MESSAGE_TYPE_KEY = 7

uint32_t robotMessageCode

uint32_t robotMessageArgument

uint8_t robotMessageTitleLength

Length of the following robotMessageTitle not including this byte

char robotMessageTitle[]

char keyTextMessage[]

Program Threads Message

The message is sent only to Primary Interface clients.

Information about all running threads might be spread into multiple messages if threads have long names. Only threads that contain labeled lines are reported. Refer to script program generated by Polyscope UI for label examples.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_ROBOT_MESSAGE = 20

uint64_t timestamp

Microseconds since controller started

int8_t source

Message Sources

uint8_t robotMessageType

ROBOT_MESSAGE_TYPE_PROGRAM_LABEL_THREADS = 14

Following structure repeats for each running program thread

→ int32_t labelId

Last executed line label id

→ uint8_t labelNameLength

→ char labelName[]

→ uint16_t threadNameLength

→ char threadName[]

Request Value Message

The message is sent only to Primary Interface clients.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_ROBOT_MESSAGE = 20

uint64_t timestamp

Microseconds since controller started

int8_t source

Message Sources

uint8_t robotMessageType

ROBOT_MESSAGE_TYPE_REQUEST_VALUE = 9

uint32_t requestId

uint32_t requestedType

Requested Types

char requestTextMessage[]

Text Message

The message is sent only to Primary Interface clients.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_ROBOT_MESSAGE = 20

uint64_t timestamp

Microseconds since controller started

int8_t source

Message Sources

uint8_t robotMessageType

ROBOT_MESSAGE_TYPE_TEXT = 0

char textMessage[]

Runtime Exception Message

The message is sent only to Primary Interface clients.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_ROBOT_MESSAGE = 20

uint64_t timestamp

Microseconds since controller started

int8_t source

Message Sources

uint8_t robotMessageType

ROBOT_MESSAGE_TYPE_RUNTIME_EXCEPTION = 10

uint32_t scriptLineNumber

uint32_t scriptColumnNumber

char runtimeExceptionTextMessage[]

Global Variable Messages

Global Variables Setup Message

The message is sent only to Primary Interface clients.

List of global variables is sent once when program starts. Afterwards update messages are sent every 100ms. If there are more variable names than can fit into one message, multiple messages will be sent with incrementing startIndex.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_PROGRAM_STATE_MESSAGE = 25

uint64_t timestamp

Microseconds since controller started

uint8_t robotMessageType

PROGRAM_STATE_MESSAGE_TYPE_GLOBAL_VARIABLES_SETUP = 0

uint16_t startIndex

char variableNames[]

List of names separated by new line character (‘\n’ character).

Example with 2 global variables: “var_1\nvar_2\n”

Global Variables Update Message

The message is sent only to Primary Interface clients.

If values can not fit into one message, multiple messages will be sent with incrementing startIndex. Order of values is matching order of variable names sent in Global Variables Setup Message.

Field

Description

Introduced in version

uint32_t messageSize

Length of overall package: total length of package including this field

uint8_t messageType

MESSAGE_TYPE_PROGRAM_STATE_MESSAGE = 25

uint64_t timestamp

Microseconds since controller started

uint8_t robotMessageType

PROGRAM_STATE_MESSAGE_TYPE_GLOBAL_VARIABLES_UPDATE = 1

uint16_t startIndex

uint8_t variableValues[]

Each variable value contains type byte, data, and terminating new line character (‘\n’ character).

Example - two variables of type BOOL=True , and STRING=”aaaa”: 0d 01 0a 03 00 04 61 61 61 61 0a

0d

01

0a

03

00

04

61

61

61

61

0a

BOOL

1=True

Separator

STRING

Length LSB

Length MSB

‘a’

‘a’

‘a’

‘a’

Separator

Data types:

Name

Value

Description

NONE

0

No content

CONST_STRING

3

uint16_t length
char string[]

VAR_STRING

4

uint16_t length
char string[]

POSE

12

float x
float y
float z
float rx
float ry
float rz

BOOL

13

uint8_t value

NUM

14

float value

INT

15

int32_t value

FLOAT

16

float value

LIST

17

uint16_t listLength
Repeated for each list element
→ uint8_t type
→ value

MATRIX

18

uint16_t nRows
uint16_t nCols
Repeated for each matrix element
→ uint8_t type
→ value

Constants

Constants used in the protocol messages.

NOTE: Unlisted values are reserved for internal use.

Control Modes

Name

Value

Description

POSITION

0

TEACH

1

FORCE

2

TORQUE

3

Robot Modes

Name

Value

Description

DISCONNECTED

0

Connection with the safety control board is not established.

CONFIRM_SAFETY

1

Robot is validating and updating the safety settings.

BOOTING

2

Safety control board is booting up and its communication with the other components is being verified.

POWER_OFF

3

Robot is ready to boot up the joints.

POWER_ON

4

Robot’s joints are booting up.

IDLE

5

Robot’s joints are ready (to go to RUNNING or BACKDRIVE modes).

BACKDRIVE

6

Robot is in back-drive mode. It is possible to move the robot in a restricted way. Brakes are being released when needed.

RUNNING

7

Brakes are fully released. Robot is ready for running a program. In Polyscope, the current safety mode is shown.

UPDATING

8

Firmware is being updated

POWERING_OFF

9

Robot arm is powering off

ARM_BOOTING

10

Robot arm is booting

ARM_UPDATING

11

Robot arm is being firmware updated

Joint Modes

Same constants are used for Tool Mode.

Name

Value

Description

RESET

235

SHUTTING_DOWN

236

BACKDRIVE

238

POWER_OFF

239

READY_FOR_POWER_OFF

240

NOT_RESPONDING

245

MOTOR_INITIALISATION

246

BOOTING

247

VIOLATION

251

FAULT

252

RUNNING

253

IDLE

255

Message Sources

Name

Value

Description

Introduced in version

JOINT_0_FPGA

100

JOINT_0_A

110

JOINT_0_B

120

JOINT_1_FPGA

101

JOINT_1_A

111

JOINT_1_B

121

JOINT_2_FPGA

102

JOINT_2_A

112

JOINT_2_B

122

JOINT_3_FPGA

103

JOINT_3_A

113

JOINT_3_B

123

JOINT_4_FPGA

104

JOINT_4_A

114

JOINT_4_B

124

JOINT_5_FPGA

105

JOINT_5_A

115

JOINT_5_B

125

TOOL_FPGA

106

TOOL_A

116

TOOL_B

126

IMMI_FPGA

107

IMMI_A

117

IMMI_B

127

TEACH_PENDANT_A

108

TEACH_PENDANT_B

118

BFB_FPGA

109

BFB_A

119

BFB_B

129

ExtenderNear_FPGA

70

ExtenderNear_MCU

71

ExtenderFar_FPGA

72

ExtenderFar_MCU

73

SCB_FPGA

40

UA

20

UB

30

ROBOTINTERFACE

-2

RTMACHINE

-3

SIMULATED_ROBOT

-4

GUI

-5

CONTROLLER

7

RTDE

8

LOGIC_PROGRAM

13

10.14.0

Message Types

Name

Value

Description

ROBOT_STATE

16

ROBOT_MESSAGE

20

MODBUS_INFO_MESSAGE

5

This message is only sent on PolyScope 5. For Polyscope X, use modbus_client_signals ROS2 topic instead.

PROGRAM_STATE_MESSAGE

25

Safety Statuses

Name

Value

Description

NORMAL

1

REDUCED

2

PROTECTIVE_STOP

3

RECOVERY

4

SAFEGUARD_STOP

5

SYSTEM_EMERGENCY_STOP

6

ROBOT_EMERGENCY_STOP

7

VIOLATION

8

FAULT

9

VALIDATE_JOINT_ID

10

UNDEFINED_SAFETY_MODE

11

AUTOMATIC_MODE_SAFEGUARD_STOP

12

SYSTEM_THREE_POSITION_ENABLING_STOP

13

TP_THREE_POSITION_ENABLING_STOP

14

IMMI_EMERGENCY_STOP

15

IMMI_SAFEGUARD_STOP

16

PROFISAFE_WAITING_FOR_PARAMETERS

17

PROFISAFE_AUTOMATIC_MODE_SAFEGUARD_STOP

18

PROFISAFE_SAFEGUARD_STOP

19

PROFISAFE_EMERGENCY_STOP

20

SAFETY_API_SAFEGUARD_STOP

22

IO_PLANE_STOP

23

Added in 10.13

Report Levels

Name

Value

Description

DEBUG

0

INFO

1

WARNING

2

VIOLATION

3

FAULT

4

CRITICAL_FAULT

5

DEVL_DEBUG

128

DEVL_INFO

129

DEVL_WARNING

130

DEVL_VIOLATION

131

DEVL_FAULT

132

DEVL_CRITICAL_FAULT

133

Requested Types

Name

Value

Description

BOOLEAN

0

Simple yes/no

INTEGER

1

Integer

FLOAT

2

A script float (a double in C++/java)

STRING

3

Text string

NONE

8

Popup

Robot Types

Name

Value

Description

UNDEFINED

0

UR5

1

Also UR7e

UR10

2

Also UR12e

UR3

3

UR3e

UR16

4

UR16e

UR18

5

UR18

UR8_LONG

6

UR8 Long

UR20

7

UR20

UR30

8

UR30

UR15

9

UR15

Tool Flange Types

Name

Value

Description

UNKNOWN

0

V1

1

V2

2

Control Box Types

Name

Value

Description

UNKNOWN

0

CB5

5

CB7

7

TP Types

Name

Value

Description

NONE

0

STANDARD

1

THREE_POSITION_ENABLING

2

Additional Resources

Product page for IMMI Module