External FTS example
It is possible to feed data of an external Force-Torque-Sensor (FTS) into the robot controller through RTDE. This feature has to be explicitly enabled by calling the URScript function ft_rtde_input_enable.
Usually, that functionality would be used with a URCap running on the robot but data can also be routed through an external computer with a matching driver for that FTS. Keep in mind that the latency introduced by the network connection may have a negative impact on the performance.
Another use case could be to inject force-torque measurements into a simulated robot for testing purposes.
This example allows setting force values that are sent to the robot as external ft measurements. The terminal user interface (TUI) is pretty simple:
Pressing the keys
x,y,z,a,b, orcwill increase the respective force/torque component by 10 (N or Nm). (a,b, andccorrespond to torques around the x, y, and z axis respectively.)Pressing the keys
X,Y,Z,A,B, orCwill decrease the respective force/torque component by 10 (N or Nm).Pressing
0will reset all force/torque components to zero.Pressing
qwill exit the program.
The example’s source code can be found in external_fts_through_rtde.cpp.
Note
This example requires the robot to be in remote control mode.
Robot initialization
The robot initialization is handed off to the ExampleRobotWrapper class:
274 g_my_robot = std::make_unique<urcl::ExampleRobotWrapper>(robot_ip, OUTPUT_RECIPE, INPUT_RECIPE, true);
275 if (!g_my_robot->isHealthy())
276 {
277 URCL_LOG_ERROR("Something in the robot initialization went wrong. Exiting. Please check the output above.");
278 return 1;
279 }
In order to use the RTDE input for the FTS, we have to enable it first by calling the
ft_rtde_input_enable function. This is done by sending a script to the robot through the
ftRtdeInputEnable() method of the UrDriver class.
281 // Enable using the force-torque input through RTDE in the robot controller
282 g_my_robot->getUrDriver()->ftRtdeInputEnable(true);
RTDE communication is moved to a separate thread in order to use the main thread for handling keyboard input commands.
Input key handling
For handling the keyboard input, define a getChar() function that reads a single character from
the terminal without waiting for a newline character. This has to be done differently on Windows
and Linux (and other unix-like systems), therefore the code is split using preprocessor directives.
38// Platform-specific implementation of getChar()
39#if defined(_WIN32) || defined(_WIN64)
40# include <conio.h>
41char getChar()
42{
43 char ch = '\0';
44 auto start_time = std::chrono::steady_clock::now();
45 while (std::chrono::duration_cast<std::chrono::seconds>(std::chrono::steady_clock::now() - start_time).count() < 1)
46 {
47 if (_kbhit())
48 {
49 ch = _getch();
50 }
51 }
52 return ch;
53}
54#else
55# include <termios.h>
56# include <unistd.h>
57# include <fcntl.h>
58# include <sys/select.h>
59char getChar()
60{
61 termios oldt, newt;
62 char ch;
63 tcgetattr(STDIN_FILENO, &oldt);
64 newt = oldt;
65 newt.c_lflag &= ~(ICANON | ECHO);
66 tcsetattr(STDIN_FILENO, TCSANOW, &newt);
67
68 int oldf = fcntl(STDIN_FILENO, F_GETFL, 0);
69 fcntl(STDIN_FILENO, F_SETFL, oldf | O_NONBLOCK);
70
71 fd_set set;
72 FD_ZERO(&set);
73 FD_SET(STDIN_FILENO, &set);
74
75 struct timeval timeout;
76 timeout.tv_sec = 1;
77 timeout.tv_usec = 0;
78
79 // Wait for input with timeout
80 int rv = select(STDIN_FILENO + 1, &set, NULL, NULL, &timeout);
81 if (rv > 0)
82 {
83 std::ignore = read(STDIN_FILENO, &ch, 1);
84 }
85 else
86 {
87 ch = '\0'; // No input
88 }
89
90 tcsetattr(STDIN_FILENO, TCSANOW, &oldt);
91 fcntl(STDIN_FILENO, F_SETFL, oldf);
92 return ch;
93}
94#endif
Setting the external force-torque values
The result from the tui function is synchonized to the RTDE communication thread using a buffer g_FT_VEC and a mutex.
200 std::scoped_lock<std::mutex> lock(g_FT_VEC_MUTEX);
201 g_FT_VEC = local_ft_vec;
237 if (g_FT_VEC_MUTEX.try_lock())
238 {
239 local_ft_vec = g_FT_VEC;
240 g_FT_VEC_MUTEX.unlock();
241 }
Note that the try_lock() method is used in the RTDE thread to avoid blocking the thread if the
tui thread is currently holding the lock. The new values will be available in a later cycle then.
Note
The values reported from the robot are rotated to the base coordinate system of the robot. Hence, they will not be the same as the ones sent to the robot. For them to be the same, align the TCP frame with robots base frame.
Example output
The following shows an example output. .. code:
[1760084283.005655] INFO ur_client_library/src/primary/primary_client.cpp 67: Starting primary client pipeline
[1760084283.056577] INFO ur_client_library/src/ur/dashboard_client.cpp 76: Connected: Universal Robots Dashboard Server
[1760084283.060021] INFO ur_client_library/src/example_robot_wrapper.cpp 201: Robot ready to start a program
[1760084283.060652] INFO ur_client_library/src/helpers.cpp 95: SCHED_FIFO OK, priority 99
[1760084283.061806] INFO ur_client_library/src/rtde/rtde_client.cpp 139: Negotiated RTDE protocol version to 2.
[1760084283.061944] INFO ur_client_library/src/rtde/rtde_client.cpp 291: Setting up RTDE communication with frequency 500.000000
Program running: false
[1760084284.095662] INFO ur_client_library/src/primary/primary_client.cpp 67: Starting primary client pipeline
[1760084284.225584] INFO ur_client_library/src/control/reverse_interface.cpp 225: Robot connected to reverse interface. Ready to receive control commands.
Program running: true
Press x,y,z to increase the respective axes, 0 for reset, q for quit.
[1760084284.225944] INFO ur_client_library/src/helpers.cpp 95: SCHED_FIFO OK, priority 99
[1760084284.227630] INFO ur_client_library/src/control/reverse_interface.cpp 238: Connection to reverse interface dropped.
Program running: false
Force-torque reported by robot: [0, 0, 0, 0, 0, 0]
Force-torque reported by robot: [0, 0, 0, 0, 0, 0]
<'x' pressed>
Artificial FT input: [10, 0, 0, 0, 0, 0]
Press x,y,z to increase the respective axes, 0 for reset, q for quit.
<'y' pressed>
Artificial FT input: [10, 10, 0, 0, 0, 0]
Press x,y,z to increase the respective axes, 0 for reset, q for quit.
<'y' pressed>
Artificial FT input: [10, 20, 0, 0, 0, 0]
Press x,y,z to increase the respective axes, 0 for reset, q for quit.
Force-torque reported by robot: [10, 20, 2.05103e-09, 0, 0, 0]
Force-torque reported by robot: [10, 20, 2.05103e-09, 0, 0, 0]
Force-torque reported by robot: [10, 20, 2.05103e-09, 0, 0, 0]
Force-torque reported by robot: [10, 20, 2.05103e-09, 0, 0, 0]
<'Y' pressed>
Artificial FT input: [10, 10, 0, 0, 0, 0]
Press x,y,z to increase the respective axes, 0 for reset, q for quit.
Force-torque reported by robot: [10, 10, -3.67436e-15, 0, 0, 0]
Force-torque reported by robot: [10, 10, -3.67436e-15, 0, 0, 0]
<'c' pressed>
Artificial FT input: [10, 10, 0, 0, 0, 10]
Press x,y,z to increase the respective axes, 0 for reset, q for quit.
Force-torque reported by robot: [10, 10, -3.67436e-15, 2.05104e-09, -2.05103e-09, 10]
<'X' pressed>
Artificial FT input: [0, 10, 0, 0, 0, 10]
Press x,y,z to increase the respective axes, 0 for reset, q for quit.
Force-torque reported by robot: [2.05103e-09, 10, 2.05103e-09, 2.05104e-09, -2.05103e-09, 10]
<'0' pressed>
Artificial FT input: [0, 0, 0, 0, 0, 0]
Press x,y,z to increase the respective axes, 0 for reset, q for quit.
Force-torque reported by robot: [0, 0, 0, 0, 0, 0]
Force-torque reported by robot: [0, 0, 0, 0, 0, 0]
<'q' pressed>
Artificial FT input: [0, 0, 0, 0, 0, 0]
[1760084296.656255] INFO ur_client_library/src/primary/primary_client.cpp 61: Stopping primary client pipeline