DashboardClient
The DashboardClient
wraps the calls on the Dashboard server
directly into C++ functions.
After connecting to the dashboard server by using the connect()
function, dashboard calls can be
sent using the sendAndReceive()
function. Answers from the dashboard server will be returned as
string from this function. If no answer is received, a UrException
is thrown.
Some functions are also wrapped into command...()
functions such as
commandCloseSafetyPopup()
. These functions are blocking and will wait for the necessary action
being done. This can involve querying another call to the dashboard server until the action is
done. For example, commandPowerOn()
will block until the robot reports “Robotmode: RUNNING” or
the given timeout is reached.
The dashboard_example.cpp shows how to use this class:
61 auto my_dashboard = std::make_unique<DashboardClient>(robot_ip);
62 if (!my_dashboard->connect())
63 {
64 URCL_LOG_ERROR("Could not connect to dashboard");
65 return 1;
66 }
67
68 if (!my_dashboard->commandPowerOff())
69 {
70 URCL_LOG_ERROR("Could not send power off");
71 return 1;
72 }
73
74 // Get the PolyScope version
75 std::string version;
76 my_dashboard->commandPolyscopeVersion(version);
77 URCL_LOG_INFO(version.c_str());
78
79 my_dashboard->commandCloseSafetyPopup();