Trajectory Point Interface

The TrajectoryPointInterface allows sending trajectory points to the robot. It is intended to be used in conjunction with the ReverseInterface during trajectory forwarding.

Communication regarding trajectory point execution would usually look like this:

Trajectory interface

Basically, the TrajectoryPointInterface transfers the trajectory points from the external control PC to the robot for execution. Execution isn’t started, before a start command is sent via the ReverseInterface. Once trajectory execution is done (either successful, failed or canceled externally), the robot will send a response back to the control PC via the trajectory socket.

Note

The TrajectoryPointInterface simply forwards the trajectory points to the robot. Execution is done using respective URScript functions such as movej or movel. Therefore, all parameters and restrictions of these functions apply. For example, velocity and acceleration parameters will be ignored if there is a time > 0 given.

Communication protocol

The TrajectoryPointInterface’s “trajectory_socket” on the robot is expecting 32 bit integer representations in 21 datafields. The data fields have the following meaning:

Table 13 trajectory_socket message format

index

meaning

0-5

trajectory point positions (Multiplied by MULT_JOINTSTATE)

6-11

trajectory point velocities (Multiplied by MULT_JOINTSTATE). For MOVEC, this contains the “via pose”.

12-17

trajectory point accelerations (Multiplied by MULT_JOINTSTATE).

For MOVEC:

  • 12: velocity (Multiplied by MULT_JOINTSTATE)

  • 13: acceleration (Multiplied by MULT_JOINTSTATE)

  • 14: mode (Multiplied by MULT_JOINTSTATE)

18

trajectory point type

  • 0: MOVEJ

  • 1: MOVEL

  • 2: MOVEP

  • 3: MOVEC

  • 51: SPLINE)

19

trajectory point time (in seconds, multiplied by MULT_TIME)

20

depending on trajectory point type

  • MOVEJ, MOVEL, MOVEP and MOVEC: point blend radius (in meters, multiplied by MULT_TIME)

  • SPLINE: spline type (1: CUBIC, 2: QUINTIC)

where

  • MULT_JOINTSTATE: 1000000

  • MULT_TIME: 1000