Get the raw numeric value of a value object converted into another compatible unit as a string
The returned value is formatted using FixedPointNumber#getDisplayValue and is without any unit symbols or label
const value = { value: 1, unit: "m/s" }; const toUnit = "mm/s"; const convertedValue = valueRawConverter(value, toUnit); console.log(convertedValue); // outputs "1000"
Error if the value object and the provided unit are incompatible
The raw numeric value of the converted value object as a formatted string
convertValue
The value object to be converted
The unit to convert into, must be compatible with the value object's unit
Generated using TypeDoc
Get the raw numeric value of a value object converted into another compatible unit as a string
The returned value is formatted using FixedPointNumber#getDisplayValue and is without any unit symbols or label
Example
Throws
Error if the value object and the provided unit are incompatible
Returns
The raw numeric value of the converted value object as a formatted string
See
convertValue