3. Project Management
3.1. Create a New Project
Open the main menu by clicking the hamburger icon in the top-left corner.
Hamburger menu options
Select New Project.
Choose one of the following options:
Empty Project (blank workspace)
Template (e.g., Palletizing, Pick & Place, Machine Tending)
New Project menu
3.2. Open an Existing Project
To open an existing project, open the main menu and choose Open Project. Then browse and select the desired project file.
Open Project Dialog
3.3. Save and Load Projects
Click Save As to download the project file locally with the name simProject.urz.
Modify the file name if needed.
Save your project to your local file
To reload, use Open Project and select the file.