10. Shadow Programming
Shadow programming enables robot programming using a preview, eliminating the need for physically moving to target points.
Create Move commands without jogging the robot.
Teach points by selecting positions in the scene.
Save and execute the program.
Teaching a point in a Move
Robots can be programmed in preview mode without activating the motors.
Move the shadow of the robot to the desired position