Auto Annotation for object detection

Warning

The AI Accelerator requires ROS 2 Humble, so PolyScope X 10.12.1 is the latest compatible release. PolyScope X 10.13 and later use ROS 2 Jazzy and are not currently supported.

The Auto Annotation tool records a short camera sequence of the part you want to detect, lets you annotate the first frame, propagates that annotation through the sequence, and writes a COCO dataset used to train an RT-DETR detector. Training, loading, and testing are done from the companion Console UI that launches with this tool.

All paths below are inside the SDK container, under /workspaces/isaac_ros-dev/ (host-side equivalent is typically ~/aia_sdk/ros/... depending on your mount).

End-to-end flow (summary)

Stage

Where

Action

What gets written

1. Record

Auto Annotation UI

Press R

data/videos/video_N/*.jpeg

2. Load

Auto Annotation UI

Press L

(reads last video_N; no new files)

3. Annotate frame 0

Auto Annotation UI

Left/right click

Prompt points in memory only

4. Propagate

Auto Annotation UI

Press P

Masks/boxes in memory; also auto-writes COCO under data/datasets/rtdetr_active/

5. Review

Auto Annotation UI

Press V

Playback only

6. (Optional) Regenerate COCO

Auto Annotation UI

Press G

Rewrites the same COCO train/validation files

7. Train

Console UI

Train model

data/models/rtdetr_active/checkpoint-*

8. Load

Console UI

Load model

Loads highest-numbered checkpoint-* into RT-DETR (no new folder)

9. Test

Console UI

Detect

Inference overlays / terminal logs

        flowchart TB
    rec["<b>1. Record</b> — R"]
    ann["<b>2-3. Annotate</b> — L + clicks"]
    prop["<b>4. Propagate</b> — P"]
    train["<b>6. Train model</b>"]
    loadm["<b>7. Load model</b>"]
    detect["<b>8. Detect</b>"]

    rec -- "video_N/*.jpeg" --> ann --> prop
    prop -- "coco_train.json + coco_validation.json" --> train
    train -- "checkpoint-&lt;step&gt;" --> loadm --> detect
    prop -. "5. Review with V" .-> ann

    classDef annotstep fill:#FFFFFF,stroke:#002B39,stroke-width:1.5px,color:#002B39
    classDef consolestep fill:#D7DDDF,stroke:#002B39,stroke-width:1.5px,color:#002B39
    class rec,ann,prop annotstep
    class train,loadm,detect consolestep
    

White boxes are steps in the Auto Annotation window, shaded boxes are buttons in the Console UI, and the edge labels are the files each stage leaves on disk.

Steps to launch

Enter the SDK container as described in the SDK article:

cd ~/aia_sdk/ros
./scripts/run_sdk_setup.sh

Inside the container run:

./scripts/run_tool_auto_annotation.sh

This launches the Auto Annotation tool and the Console UI.

Auto Annotation tool window next to the Console UI after launch

The Auto Annotation tool (left) and the Console UI (right) both start from run_tool_auto_annotation.sh. Annotation happens in the Auto Annotation window; training and loading happen in the Console UI.

Stage 1 — Record video frames (R)

  1. Aim the camera at the part. Make sure the part is fully in view when you start.

  2. Press R to start recording.

  3. Capture multiple viewpoints of the stationary part by moving the robot (Freedrive or gentle programmed motion) so the camera orbits or approaches the part.

  4. Press R again to stop.

Tip

Prefer moving the robot, not the part. Hands, gloves, or a person moving the object often end up in the frames and get learned as part of the object. Leave the part fixed on the table and move the robot/camera instead for a short, clean clip.

Keep the clip short (under ~10 seconds). Longer sequences make propagation much slower (can exceed 1 hour).

Auto Annotation window while recording frames from the camera

Recording in progress after pressing R. Each frame is written as a sequential JPEG into a new data/videos/video_<N>/ folder.

Files generated

data/videos/video_<N>/
  000000.jpeg
  000001.jpeg
  000002.jpeg
  ...
  • <N> is the next free integer (video_0, video_1, …).

  • Frames are sequential JPEGs (not a single .mp4).

Stage 2 — Load the recording (L)

Press L to load the last recorded video_N folder. The first frame appears for annotation.

Press SPACE any time to return to the live camera feed.

First frame of the loaded recording shown in annotation mode

Annotation mode after pressing L: the first frame of the last recording is frozen and ready for prompt points. Press SPACE to go back to the live feed.

Files generated

None. This only reads data/videos/video_<N>/.

Stage 3 — Annotate the first frame

On the first frame:

  • Left click — positive prompt (this is the part). Place one or more green points on the object.

  • Right click — negative prompt (this is not the part). Mark all unwanted regions that the mask might otherwise include: table surface, wall, fixtures, shadows, neighbouring objects, robot links if visible, and any leftover hand/glove pixels.

  • Click an existing point again to remove it.

Refine until the highlight covers only the part. If the magenta/green overlay spills onto the table or background, add more negative points there before you propagate.

Auto Annotation with green positive points on the part and red negative points on table and wall

Example annotation: green positive points on the part, red negative points on unwanted regions (table, wall, and other background). Keep adding negatives until the mask stays on the object only.

Positive prompt point placed on the part, highlighting the segmentation

Left click adds a positive prompt point. The highlighted region is what SAM2 currently considers the part.

Negative prompt point excluding background from the segmentation

Right click adds a negative prompt point to shrink the highlight back off the background or neighbouring objects.

Files generated

None. Prompt points stay in memory until you propagate.

Stage 4 — Propagate annotations (P)

Press P to propagate the first-frame annotation through every frame (SAM2). This can take several minutes.

When propagation finishes successfully, the tool automatically generates the COCO dataset (same output as pressing G).

Files generated (automatic COCO write)

data/datasets/rtdetr_active/
  train/
    000000.jpeg          # ~80% of frames (copied from video_N)
    ...
    coco_train.json      # COCO annotations for train images
  validation/
    00000N.jpeg          # remaining ~20% of frames
    ...
    coco_validation.json # COCO annotations for validation images

Notes:

  • Images are copied from data/videos/video_N/ into train/ and validation/ (80/20 split by sorted filename order).

  • Each JSON lists images, bounding boxes / segmentation from the propagated masks, and a single category (object).

  • This dataset is what Train model reads. Without these files, training fails.

Stage 5 — Review segmentation (V)

Press V to play the segmented video and confirm the highlight stays on the part for every frame.

Segmented playback starting after pressing the V key

Segmented playback started with V. The propagated mask is drawn on every frame of the recording.

Later playback frame with the mask still tracking the part

A later frame in the same playback. The mask should stay on the part for the whole clip; if it drifts or disappears, re-annotate and propagate again.

Files generated

None required for training. If review looks wrong, re-annotate and press P again (COCO will be regenerated).

Stage 6 — (Optional) Regenerate COCO (G)

Press G to rewrite the COCO dataset from the current propagation result. Use this if you need to regenerate coco_train.json / coco_validation.json without re-propagating, or if automatic generation after P did not succeed.

Files generated

Same layout as Stage 4:

data/datasets/rtdetr_active/train/coco_train.json
data/datasets/rtdetr_active/train/*.jpeg
data/datasets/rtdetr_active/validation/coco_validation.json
data/datasets/rtdetr_active/validation/*.jpeg

Stage 7 — Train model (Console UI → Train model)

With COCO present under data/datasets/rtdetr_active/, use the separate Console UI window (Detection: rtdetr_active):

  1. Click Train model.

  2. Watch the terminal: it verifies the COCO files, then runs HuggingFace training for many epochs (several minutes or longer).

  3. Wait until training finishes (look for training-complete / end logs). Do not interrupt the container mid-train.

Console UI in detection mode with the Train model button highlighted

Train model in the Console UI (Detection: rtdetr_active). The terminal reports the verified COCO files and the train/validation image counts as training starts.

Training reads:

data/datasets/rtdetr_active/train/coco_train.json
data/datasets/rtdetr_active/validation/coco_validation.json

and fine-tunes from the base RT-DETR weights under Isaac assets (isaac_ros_assets/models/rtdetr/...).

Files generated (checkpoint-*)

data/models/rtdetr_active/
  checkpoint-<step>/     # e.g. checkpoint-750
    config.json
    model.safetensors    # or pytorch_model.bin
    preprocessor_config.json
    training_args.bin
    trainer_state.json
    optimizer.pt
    scheduler.pt
    ...                  # other HuggingFace Trainer artifacts
  checkpoint-<older>/    # earlier save; only a few are kept
  • The folder name is checkpoint- plus the training step number (not a version you choose).

  • Trainer saves periodically (per epoch) and keeps a limited number of folders (save_total_limit).

  • Use the highest-numbered folder that completed successfully (Console UI Load model picks this automatically).

There is no separate manual “create checkpoint” step — Train model is what creates checkpoint-*.

Stage 8 — Load model (Console UI → Load model)

Click Load model. The UI finds the highest-numbered checkpoint-* under data/models/rtdetr_active/ and loads it into the detector.

Console UI in detection mode with the Load model button highlighted

Load model loads the highest-numbered checkpoint-* from data/models/rtdetr_active/. Wait for the terminal to confirm the load before running inference.

Files generated

None. The existing checkpoint folder is loaded into memory.

For robot programs, point URScript at the same folder relative to data/models/:

ark_load_detection_model(model="rtdetr_active/checkpoint-750")

Replace checkpoint-750 with the folder name actually present on your system.

Stage 9 — Test detection (Console UI → Detect)

  1. Place the part in camera view.

  2. Click Detect.

  3. Confirm a box (and mask, depending on pipeline) around the part in the image view; check terminal logs for class/confidence.

Console UI showing a detected object with bounding box, mask and confidence

Detect runs inference on the current frame. A correct result draws a tight box and mask on the part, with the class and confidence logged in the terminal.

Files generated

None required. This is an inference check only.

When detection looks good, continue with:

  • Detection for planar pick-and-place, or

  • Pose Estimation (needs this detector plus a textured mesh for FoundationPose).

Path cheat sheet

Paths exist in two places that point at the same files:

Where you are

Root for data files

Host (terminal on the compute module desktop)

~/aia_sdk/ros/

SDK Docker container

/workspaces/isaac_ros-dev/

Where generated files live

Stage

What is created

Host path

Container path

Record (R)

Frame JPEGs

~/aia_sdk/ros/data/videos/video_<N>/

/workspaces/isaac_ros-dev/data/videos/video_<N>/

Propagate scratch

Temporary SAM2 frame

~/aia_sdk/ros/data/tmp_video_dir/

/workspaces/isaac_ros-dev/data/tmp_video_dir/

Propagate / G

COCO train images + JSON

~/aia_sdk/ros/data/datasets/rtdetr_active/train/

/workspaces/isaac_ros-dev/data/datasets/rtdetr_active/train/

Propagate / G

COCO validation images + JSON

~/aia_sdk/ros/data/datasets/rtdetr_active/validation/

/workspaces/isaac_ros-dev/data/datasets/rtdetr_active/validation/

Train model

Checkpoints

~/aia_sdk/ros/data/models/rtdetr_active/checkpoint-<step>/

/workspaces/isaac_ros-dev/data/models/rtdetr_active/checkpoint-<step>/

Train model

TensorBoard / run logs

~/aia_sdk/ros/data/models/rtdetr_active/runs/

/workspaces/isaac_ros-dev/data/models/rtdetr_active/runs/

Base RT-DETR (do not delete)

Pretrained assets

~/aia_sdk/ros/isaac_ros_assets/models/rtdetr/

/workspaces/isaac_ros-dev/isaac_ros_assets/models/rtdetr/

Key files under the COCO folders:

data/datasets/rtdetr_active/train/coco_train.json
data/datasets/rtdetr_active/train/*.jpeg
data/datasets/rtdetr_active/validation/coco_validation.json
data/datasets/rtdetr_active/validation/*.jpeg

Example layout from a real compute module

After one successful annotate → propagate → train cycle, a box typically looks similar to this (counts and checkpoint numbers will differ):

~/aia_sdk/ros/data/
├── videos/
│   └── video_0/                 # e.g. ~118 frame JPEGs from recording
│       ├── 000000.jpeg
│       ├── 000001.jpeg
│       └── ...
├── tmp_video_dir/               # short-lived SAM2 scratch (safe to delete)
├── datasets/
│   └── rtdetr_active/
│       ├── train/               # e.g. ~94 images + coco_train.json
│       └── validation/          # e.g. ~24 images + coco_validation.json
└── models/
    └── rtdetr_active/
        ├── checkpoint-564/      # older save (~490 MB each)
        ├── checkpoint-2350/     # highest number = what Load model uses
        └── runs/                # training logs only

Quick checks from a host terminal on the compute module:

# List recordings
ls ~/aia_sdk/ros/data/videos/

# Confirm COCO files exist
ls ~/aia_sdk/ros/data/datasets/rtdetr_active/train/coco_train.json
ls ~/aia_sdk/ros/data/datasets/rtdetr_active/validation/coco_validation.json

# See which checkpoints are available (Load model picks the highest number)
ls -d ~/aia_sdk/ros/data/models/rtdetr_active/checkpoint-*

# Disk use
du -sh ~/aia_sdk/ros/data/videos \
       ~/aia_sdk/ros/data/datasets \
       ~/aia_sdk/ros/data/models/rtdetr_active

Inside the container, use the same relative paths under /workspaces/isaac_ros-dev/.

Clean up files and retrain

Stop Auto Annotation / Console UI and any detection example first. Prefer deleting from the host (not inside the container). See also the broader cleanup guidance in Clean up data files.

What is safe to delete vs keep

Goal

Delete these (host paths)

Keep

Free disk after a good train

data/videos/, data/tmp_video_dir/, data/models/rtdetr_active/runs/, unused older checkpoint-*

The checkpoint your program loads; datasets/rtdetr_active/ if you may retrain

Start annotation over (same part, new recording)

data/videos/, data/tmp_video_dir/

Optional: keep old COCO until new P/G rewrites it

Full retrain from scratch

data/videos/, data/tmp_video_dir/, data/datasets/rtdetr_active/, data/models/rtdetr_active/checkpoint-*, data/models/rtdetr_active/runs/

Base Isaac assets under isaac_ros_assets/models/

Never delete

—

isaac_ros_assets/models/ (except models_backup), config/config.yaml, launch/scripts

Light cleanup (recordings and scratch only)

Safe after COCO already exists under datasets/rtdetr_active/ (frames were copied there during P / G):

rm -rf ~/aia_sdk/ros/data/videos \
       ~/aia_sdk/ros/data/tmp_video_dir

rm -rf ~/aia_sdk/ros/data/models/rtdetr_active/runs

Keep the latest checkpoint, remove older ones

If disk is tight but detection already works:

# Example: keep checkpoint-2350, remove older checkpoint-564
rm -rf ~/aia_sdk/ros/data/models/rtdetr_active/checkpoint-564

Confirm with ls -d ~/aia_sdk/ros/data/models/rtdetr_active/checkpoint-* before and after.

Keyboard reference (Auto Annotation UI)

Key

Action

R

Start/stop recording

L

Load last recording

SPACE

Resume live camera feed

Left / right click

Positive / negative prompt on first frame

P

Propagate annotation (+ auto COCO generation)

V

View segmented playback

G

Regenerate COCO dataset

Q

Quit

Common issues

Recording and annotation

Symptom

Likely cause

What to do

R does nothing / no new video_N

Camera not streaming or tool not fully started

Confirm the Auto Annotation window shows the live feed. Restart ./scripts/run_tool_auto_annotation.sh. Check camera / ROS domain settings in SDK config.yaml.

Recording folder empty or very few frames

Clip stopped immediately, or camera dropped frames

Record again; keep the part in view the whole time. Aim for under ~10 seconds but more than a few frames.

Mask covers background or the wrong object

Weak / missing negative prompts

Add right-click negatives on all unwanted regions (table, wall, fixtures, shadows); re-propagate (P), review with V.

Mask drifts or disappears mid-clip (V)

Hard motion, occlusion, or hands in frame

Re-record by moving the robot with the part fixed (no hands in view); annotate carefully with positives + negatives; P again.

Propagation (P) takes extremely long

Recording too long

Keep clips under ~10 seconds. Delete long video_N folders and record a shorter one.

Hands / person appear in the trained detector

Part was moved by hand during R

Prefer robot/camera motion with a stationary part. Clean dataset and retrain.

COCO dataset / Train model

Symptom

Likely cause

What to do

Train model fails / missing images

coco_*.json missing or image paths do not match files on disk

Confirm both JSON files exist (see Path cheat sheet). Re-run P or G.

Train starts then errors on empty dataset

Propagate never finished or G was never successful

Watch terminal for COCO write messages after P. Verify train/ and validation/ contain both JPEGs and JSON.

Training never creates checkpoint-*

Interrupted mid-train or container stopped

Re-run Train model and wait for completion logs. Do not close the container.

Old bad labels keep coming back

You retrained without clearing datasets/rtdetr_active/

Do a full clean and retrain.

Quick integrity check from the host:

ls ~/aia_sdk/ros/data/datasets/rtdetr_active/train/coco_train.json \
   ~/aia_sdk/ros/data/datasets/rtdetr_active/validation/coco_validation.json

# Counts should be non-zero (example after one good run: ~94 train, ~24 val)
ls ~/aia_sdk/ros/data/datasets/rtdetr_active/train/*.jpeg | wc -l
ls ~/aia_sdk/ros/data/datasets/rtdetr_active/validation/*.jpeg | wc -l

Load model / Detect

Symptom

Likely cause

What to do

Load model cannot find a checkpoint

No checkpoint-<number> under data/models/rtdetr_active/

Finish Train model, then ls -d ~/aia_sdk/ros/data/models/rtdetr_active/checkpoint-*.

Detect misses the part or is unstable

Dataset too small / poor viewpoints, or wrong checkpoint loaded

Record more angles, clean and retrain, then Load model again.

Robot program loads a different model than the Console UI

Hard-coded old checkpoint-* in URScript

Update ark_load_detection_model(model="rtdetr_active/checkpoint-...") to the folder you just trained.

Disk filling up (~500 MB per checkpoint)

Multiple checkpoint-* plus videos/ kept

Delete unused older checkpoints and data/videos/ after COCO exists (see Clean up files and retrain).

Container / tool launch

Symptom

Likely cause

What to do

Auto Annotation or Console UI blank / black

Wrong robot_serial or ros_domain_id

Fix ~/aia_sdk/ros/config/config.yaml per SDK; see Console UI blank window.

Tool fails because another example is still running

Previous Isaac container / launch still up

On the host: docker ps, then docker stop isaac_pkgs_app if needed; see Existing container not stopped.

Permission errors deleting videos/ or tmp_video_dir/

Files owned by root from inside the container

Use sudo rm -rf ... on those paths from the host, or delete from a root shell carefully.