Console UI

Warning

The AI Accelerator requires ROS 2 Humble, so PolyScope X 10.12.1 is the latest compatible release. PolyScope X 10.13 and later use ROS 2 Jazzy and are not currently supported.

The ARK Console UI is a Linux desktop GUI on the AI Accelerator compute module. Use it to view the live camera stream, capture training samples, train and load models, and run classification or detection inference without writing URScript first.

It is started automatically by several SDK example launch files (classification, detection, pose estimation, and related pipelines). Enter the SDK Docker container first:

cd ~/aia_sdk/ros
./scripts/run_sdk_setup.sh

See also SDK.

ARK Console UI in classification mode

The screenshot above shows classification mode: live camera view with the cyan ROI rectangle, status label Classification: classification_active, and the record / train / load / classify controls.

What you see in the window

Area

Description

Image view

Live camera feed from the remapped image topic. Overlays depend on mode (ROI box, 2D boxes, masks, 3D pose visuals).

Status label

Shows the active dataset/model name, e.g. Classification: classification_active or Detection: rtdetr_active.

Buttons

Mode-specific actions for recording data, training, loading models, and running inference.

Modes and launch parameters

The UI is configured by ROS 2 parameters on the console_ui node (set in each example’s launch file):

Parameter

Default

Effect

detection_flag

True

False → classification controls only. True → detection controls (and related overlays).

extended_mode

False

When True and world-model services are available, adds world-model updater buttons (trigger / retrieve pose / reset / snapshot).

use_fp

True

Selects FoundationPose-oriented detection path vs RT-DETR-only (rtdetr) when using detection features.

Examples:

  • Classification launch uses detection_flag: False (classification UI as in the screenshot).

  • Detection launch uses detection controls with use_fp: False.

  • Pose estimation / dynamic picking / full pipelines typically set extended_mode: True.

Classification controls

Shown when detection_flag is False (classification examples).

Button

What it does

Record data (state_0)

Starts/stops capturing images for class state_0 into the active classification dataset.

Record data (state_1)

Same for class state_1 (two-state classifier).

Train model

Trains a model from the recorded dataset. Can take several minutes; watch the terminal for progress (e.g. onnx conversion completed).

Load model

Loads the active model from the classification models directory.

Classify

Runs inference on the current frame using the ROI; results are printed in the terminal (class name and confidence).

Paths (inside the container)

  • Dataset: /workspaces/isaac_ros-dev/data/datasets/classification_active

  • Model: /workspaces/isaac_ros-dev/data/models/classification_active

Region of interest (ROI)

The cyan rectangle on the image is the classification ROI. Images are cropped to this region for training and inference.

  • Configure ROI in ros/config/config.yaml (roi_classification_x, roi_classification_y, roi_classification_width, roi_classification_height).

  • The UI reads these values via env_manager_node.

  • When you later run classification from the robot program, the ROI in URScript must match (see the warning on the Classification page).

Typical workflow: move the robot to the inspection pose → start the classification example → record 20–30 images per state while moving the part inside the ROI → Train model → Load model → Classify to verify.

Detection controls

Shown when detection_flag is True.

Button

What it does

Take image

Saves a still image (used when collecting samples for detection training).

Train model

Trains the active detection model (rtdetr_active).

Load model

Loads the detection model checkpoint.

Detect

Runs 2D detection (and related pipeline steps depending on launch configuration).

Detection overlays on the image view can include 2D boxes, SAM masks, and 3D pose markers when those pipeline nodes are running.

The screenshots below show the detection UI (Detection: rtdetr_active) next to the terminal output, with each step’s button highlighted.

Train model — generates the COCO dataset from the annotated recording and starts training. The terminal reports dataset generation and train/validation image counts.

Console UI with Train model selected in detection mode

Load model — loads the trained detection checkpoint from the active model directory. Wait for the terminal to confirm the model loaded before running inference.

Console UI with Load model selected in detection mode

Detect — runs inference on the current frame. Detected objects are drawn on the image view (2D box, segmentation mask, and class/confidence label), and the terminal logs detections and per-stage timing.

Console UI with Detect selected, showing a detected object with mask and confidence

Extended / world-model controls

When extended_mode is True and world-model updater services are available, additional buttons appear, for example:

  • Trigger detection — start a pose-detection update cycle

  • Retrieve pose — fetch computed part poses

  • Reset world model — clear / reset tracked parts

  • Snapshot — capture a world-model snapshot

  • Report — send perception feedback

These are used with FoundationPose / world-model pipelines (pose estimation, dynamic picking, etc.), not with the simple two-state classification UI.

How to open it

  1. Enter the SDK container as described in the SDK article:

cd ~/aia_sdk/ros
./scripts/run_sdk_setup.sh
  1. Run an example script that launches the Console UI, for example:

    • ./scripts/run_example_classification.sh

    • ./scripts/run_example_detection.sh

  2. The ARK Console UI window opens on the compute module desktop.

Troubleshooting

Black / empty image view

Usually the camera feed is not reaching console_ui. Check:

# Verify the camera is publishing (adjust namespace/topic to your setup)
ros2 topic echo /<camera>/color/image_raw --once

# Inspect what console_ui subscribes to
ros2 node info /<namespace>/console_ui

Also confirm ros_domain_id and robot serial in ros/config/config.yaml match the robot. If the camera was plugged in after the container started, restart the camera node or the example pipeline.

Buttons do nothing / services fail

The UI calls ROS 2 services (collect_image, train_model, load_model, infer_classification, wait_detection, etc.). Those services only exist while the matching example nodes are running. Always start the full example launch, not the UI alone.

Classification looks wrong after training

  • Collect more varied images inside the ROI (pose, lighting).

  • Confirm the ROI in config.yaml matches what you see in the UI and what the robot program uses.

  • Follow the guidance on the Classification page.