Hardware Manual
Warning
The AI Accelerator requires ROS 2 Humble, so PolyScope X 10.12.1 is the latest compatible release. PolyScope X 10.13 and later use ROS 2 Jazzy and are not currently supported.
A manual to guide you through initial setup of the AI Accelerator hardware is available here (a hardcopy is also provided in the box with the equipment):
https://www.universal-robots.com/manuals/EN/HTML/SW10_11/Content/Landingpages/WebPolyX/AIAcc.htm
After hardware setup, put the robot on PolyScope X 10.12.1 if it is not already, then continue with Centercode (downloads and version check), then the SDK installation. On the robot, that includes installing aia_core-2.1.33.urcapx, orbbec-gemini-v335Lg-1.3.10.urcapx, and aia-sdk-6.6.10.urcapx — see Install URCapX on the robot.