Troubleshooting
Warning
The AI Accelerator requires ROS 2 Humble, so PolyScope X 10.12.1 is the latest compatible release. PolyScope X 10.13 and later use ROS 2 Jazzy and are not currently supported.
Pick the issue that matches what you see, then open that page. Paths below assume a 2.x compute module: host ~/aia_sdk/ros/, container /workspaces/isaac_ros-dev/.
Complete SDK setup first when the problem is related to first-time install.
What are you seeing?
If you see this… |
Open this guide |
|---|---|
Setup summary shows |
|
Console UI window is black or has no camera image |
|
No camera stream in AIA Core / PolyScope, or clocks look wrong |
Utility scripts ( |
Box does not match a known-good SDK / Docker baseline |
Utility scripts ( |
Example fails while another example or terminal session is already running |
|
Disk is full, or you need to delete recordings / retrain cleanly |
|
Check CPU/GPU load, temperature, or power mode on the compute box |
|
Need to inspect the Gemini camera (RGB/depth) outside ROS |
Troubleshooting guides