[URCapX] AI Accelerator Core

Warning

The AI Accelerator requires ROS 2 Humble, so PolyScope X 10.12.1 is the latest compatible release. PolyScope X 10.13 and later use ROS 2 Jazzy and are not currently supported.

The AIA Core URCapX is the central component of the AI Accelerator platform. It provides the PolyScope X UI for configuring, deploying, and managing camera and AI features, and it coordinates communication between all system components.

Why read this guide?

This page explains what AIA Core does, the other pieces it works with, and how the components are connected. Read it once to build a mental model of the platform before you follow the setup pages.

What AIA Core does

AIA Core is a PolyScope X URCapX with an Angular frontend and a set of backend containers. Its responsibilities are:

  • Camera discovery and selection — scans the ROS 2 graph for *_camera/model_config topics and lets the operator pick the active camera(s).

  • Camera start/stop control — proxies UI actions into ROS 2 NodeControl service calls to the camera node.

  • Camera settings — persists and applies camera parameters (exposure, IR, laser).

  • Hand-eye calibration — a chessboard workflow backed by a FastAPI studio service and a dedicated ROS 2 calibration node. The result is saved to /etc/aix_cameras/camera.yaml and published as a PolyScope frame.

Platform components

The AI Accelerator is made of three cooperating URCapX / stacks. AIA Core is the control plane; the camera URCap owns the sensor; pandai_ark runs the AI (NVIDIA Isaac ROS on the Jetson — see How PandaI uses NVIDIA Isaac).

Component

Role

Runs on

aia_core_urcap (this page)

Camera configuration, selection, control, and hand-eye calibration

AI Accelerator compute box

Camera Creator (camera_creator_urcap)

Orbbec camera lifecycle: starts/stops the ROS 2 driver, advertises the camera

AI Accelerator compute box

pandai_ark (ARK stack)

Perception (RT-DETR, SAM, FoundationPose), world model, planning, web bridge

AI Accelerator compute box (GPU)

All three run on the AI Accelerator compute box (embedded NVIDIA Jetson Orin AGX 64GB). The frontends run in the PolyScope X teach-pendant browser on the robot controller.

How the pieces connect

AIA Core URCapX with Calibration, Settings, and Camera Manager, associated with the Camera Creator ROS service and the Pandai ARK AI modules

Figure 1AIAC: Overview of the system components used by the AIA Core URCapX. AIA Core (with its frontend, calibration, and settings) drives a Camera Manager that is associated with the Camera Creator (a ROS service) and the Pandai ARK AI modules, each in its own docker container.

The teach pendant hosts the Angular UIs. The compute box hosts the backends, the camera driver, and the ARK perception stack. The frontends talk to their backends over HTTP/WebSocket; everything on the compute box talks over ROS 2. The diagram below expands Figure 1AIAC into the concrete containers, ports, and ROS 2 interfaces.

        flowchart TB
    subgraph PENDANT["PolyScope X teach pendant (browser)"]
        aiafe["<b>AIA Core frontend</b><br/>Angular"]
        camfe["<b>Camera Creator frontend</b><br/>Angular + URScript preamble"]
        urctrl["<b>URControl</b><br/>robot program"]
    end

    subgraph BOX["AI Accelerator compute box (Jetson Orin AGX 64GB)"]
        subgraph CORE["aia_core_urcap"]
            flask["<b>aia-core-backend</b><br/>Flask :35000"]
            studio["<b>calib_studio-backend</b><br/>FastAPI :35001"]
            calib["<b>aia-calib-backend</b><br/>hand-eye node + bridge :30018"]
            sel["<b>camera-selector-service</b><br/>SelectCamera"]
        end
        subgraph CAM["camera_creator_urcap"]
            camsvc["<b>CameraNodeService</b><br/>NodeControl / NodeInfo / NodeList"]
            orbbec["<b>Orbbec driver</b><br/>gemini_330_series"]
        end
        subgraph ARK["pandai_ark"]
            pipe["<b>pipeline_image_node</b><br/>RT-DETR + SAM + FP"]
            wm["<b>world_model_updater</b>"]
            arkbridge["<b>ur-ros2-web-bridge</b><br/>:30017"]
        end
    end

    aiafe -- "HTTP :35000" --> flask
    aiafe -- "WebSocket :35001" --> studio
    aiafe -- "WebSocket :30018" --> calib
    camfe -- "UR Contribution API" --> urctrl
    urctrl -- "ROS 2 NodeControl" --> camsvc

    flask -- "ROS 2 SelectCamera" --> sel
    flask -- "ROS 2 NodeControl" --> camsvc
    flask -. "ROS 2 sub: model_config" .-> camsvc

    camsvc -- "ros2 launch" --> orbbec
    orbbec -- "color / depth / camera_info" --> pipe
    orbbec -- "color + camera_info" --> calib

    pipe -- "process_image" --> wm
    arkbridge -- "pub/sub/srv relay" --> ARK
    PENDANT -- "WebSocket :30017" --> arkbridge

    classDef pendant fill:#D7DDDF,stroke:#002B39,stroke-width:1.5px,color:#002B39
    classDef core fill:#FFFFFF,stroke:#002B39,stroke-width:1.5px,color:#002B39
    classDef cam fill:#F7F8F7,stroke:#8FA3AB,stroke-width:1px,color:#33484F
    classDef ark fill:#EDF1F2,stroke:#002B39,stroke-width:1.5px,color:#002B39
    class aiafe,camfe,urctrl pendant
    class flask,studio,calib,sel core
    class camsvc,orbbec cam
    class pipe,wm,arkbridge ark
    

The registration handshake that lets AIA Core auto-discover a camera is described on the Camera Creator page.

Containers and ports

AIA Core is deployed as four containers (from aia_core_urcap/aia-core/manifest.yaml):

Container

Image

Port(s)

Protocol

Notes

aia-core-backend

aia-core-backend:latest

35000

HTTP

Flask REST API; ROS 2 camera discovery and control

calib_studio-backend

calib_studio-backend:latest

35001

WebSocket

FastAPI calibration studio; robot motion; waypoints

aia-calib-backend

aia-calib-backend:latest

30018 (bridge), 8080 (health)

WebSocket / HTTP

Hand-eye calibration node + web bridge; host network, privileged

camera-selector-service

camera-selector-service:latest

—

ROS 2

Implements pandai_camera_selection_service

Communication paths

From

To

Mechanism

Purpose

AIA Core frontend

aia-core-backend

HTTP :35000

Camera discovery, selection, start/stop

AIA Core frontend

calib_studio-backend

WebSocket :35001

Robot motion, waypoints, calibration save

AIA Core frontend

aia-calib-backend bridge

WebSocket :30018

Calibration service calls, TF subscribes

aia-core-backend

camera-selector-service

ROS 2 SelectCamera

Set the active camera(s)

aia-core-backend

Camera Creator

ROS 2 NodeControl

Start / stop / restart the camera node

aia-core-backend

Camera Creator

ROS 2 topic (subscribe)

{ns}_camera/model_config discovery

Camera driver

pandai_ark perception

ROS 2 topics

color/image_raw, depth/image_raw, camera_info

Persistent files

AIA Core keeps state on two mounts inside its containers:

  • /mount (persistent) — waypoints and server_ip.txt (remote-control flag).

  • /etc (permanent) — hand-eye calibration at /etc/aix_cameras/camera.yaml (plus a .backup). This is the file to retrieve after calibration; it can also be read via the calib studio API (/get_calibration_info, /get_camera_calibration/<name>).

PolyScope tabs

Screenshots of the AIA Core tabs (Calibration, Setup, Results) and a short description of each will go here.

Installation

Install the following URCapX files on the PolyScope X robot, in this order. Full steps (USB and install-urcap) are in SDK — Install URCapX on the robot.

File

Role

aia_core-2.1.33.urcapx

This URCapX (Core UI, camera manager, calibration)

orbbec-gemini-v335Lg-1.3.10.urcapx

Kit camera (Gemini 335Lg)

aia-sdk-6.6.10.urcapx

SDK URScript API used by the examples

Download the files from Centercode. The NVIDIA Isaac SDK still installs on the compute module as a .deb — that is separate from these robot packages.

Official documentation

Link to downloadable PDF documentation from the UR website.